(1)| 12/23/2005 10:28 AM | |
|
Joined: 8/31/2005 Last visit: 1/7/2026 Posts: 217 Rating:
|
Hi Shaun! The standard way to get data out of the S7 to a PC is via OPC. From OPC you can put the data where you want. Have a look at these applications: Connection of Databases via open Interfaces Using OPC-XML, Programmed in C# .net This application talks about WinAC RTX, a software PLC, but it is the same for hardware PLC like S7-300 or S7-400 (this application also uses the OPC-XML interface, which enables you to access data from the S7 PLC over the web) Or: OPC: Mass Data Acquisition with an OPC Client in C# based on .NET This application uses the most common OPC-DA interface. All these applications use Industrial Ethernet for the communication between PLC and PC but PROFIBUS can be used in the same way. |
Last edited by: Chris at: 12/23/2005 10:29 AMGreetings, Chris |
|
This contribution was helpful to
|
|
Follow us on