8/27/2014 4:43 PM | |
Joined: 5/12/2006 Last visit: 9/16/2025 Posts: 22710 Rating:
|
Hi, WTF? This are no Inverters! You can't go Online to this Parts ! A Inverter which you can connect to is SINAMICS S120 (CU320) or SIMOTION D (D425). All parts you have listed in this thread are MotorModules or Sensor Modules which are connected with DRIVE-CLiQ to a Control Unit, with such a Control Unit you can go online. The Motormodules or Sensormodules have no Online Interface like Ethernet or PROFIBUS, only the DQ Interface. here you can download the manuals for the sinamics system. Please read this manuals . Regards |
Follow us on