9/4/2014 9:44 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating:
|
Excuse my bad english. In the appendix an example. |
This contribution was helpful to
1 thankful Users |
9/4/2014 9:48 PM | |
Posts: 24 Rating:
|
Thank you 190B |
This contribution was helpful to
1 thankful Users |
9/6/2014 7:02 PM | |
Posts: 24 Rating:
|
I tried in this way, but so the system is activated according to the value set without taking into consideration the value it receives from the probe. have any suggestion? thank Attachmenttest.zip (339 Downloads) |
9/6/2014 8:53 PM | |
Posts: 5225 Rating:
|
Hi there. 190B has provided a brilliant piece of coding to explain how a setpoint can be created. One of the counters at the end of the circuit could be used as a setpoint number. I am providing a simplified method built onto the method you have provided. In this design I have also a counter to provide a setpoint that is adjusted via I1 and I2 (digital inputs). You will see that the counter feeds into a compare function. Also going into the the compare function is an analog signal. This design does not attempt to do the correct signal conditioning and it provides for a very rough adjustment (10 increments and with multiplier). I am not trying to give you the whole design. I am only trying to give you design direction. I would strongly advise you to make use of the consept that 190B has provded to make a a setpoint and combining with what I provide. I am unsure to what you are using as a "probe". It can mean so many things. Kindly provide more information if you are giving feedback to ask for more help. Good luck with your design. w Attachmenttest (modify1).zip (368 Downloads) |
This contribution was helpful to
1 thankful Users |
9/6/2014 9:18 PM | |
Posts: 24 Rating:
|
HiWilliam B., thanks for your code, I try it Ferdinando
|
This contribution was helpful to
1 thankful Users |
Follow us on