9/11/2014 2:03 PM | |
Joined: 1/30/2007 Last visit: 9/8/2025 Posts: 89 Rating:
|
Have you tried with the setpoint set to Actual position of the Master, instead of Command position? |
9/11/2014 3:20 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, when it is possible to synchronise in standstill, it is possible touse "Fixed Gear" 2.1 Fixed Gear http://support.automation.siemens.com/WW/view/en/98993534 |
With best regards, |
|
9/12/2014 10:57 AM | |
Posts: 153 Rating:
|
You may want to also try the _enablegearing command. Even easier would be the PLC Open MC_Gearing.. These work well, as long as you have a GEAR license. |
Follow us on