10/7/2014 10:46 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hi please find information behind Link: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=21901735&lang=de&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=4000024&treeLang=de It is possible to work with sharde device SIMOTION/SIMATIC or I-device .... |
With best regards, |
|
10/8/2014 12:21 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating:
|
The proposed link : https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=21901735&lang=de&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=4000024&treeLang=de does not work. Does that mean f.i. when I have a S7 profinet CPU and Simotion that is connected to the same profinet network, that if there is an ET200M on that profinet, that one IO-card of the ET200M can be read by the S7 CPU and another IO-card on the same ET200M could be read by the Simotion? Or is it even possible that both read the same IO-card? |
10/8/2014 12:25 PM | |
Joined: 5/12/2006 Last visit: 9/17/2025 Posts: 22710 Rating:
|
Hello, no the same IO-Card is not possible. The first case , one IO-Card to one PLC is possible. Regards Christoph |
Follow us on