(0)| 11/13/2007 6:30 AM | |
|
Posts: 22 Rating:
|
Dear All, I have a system in which I am using S7-300 CPU 315-2DP Telecontrol Moddule VICOS RTU TIM 3V BN (MLFB No. 6NH7808-3AA00) with some remote I/O & profibus network . Now I want to upgrade the system to S7-300 software redudedant. (S7-300 R) using siemens software FB's. I considered two CPU 315 - 2DP IM153-2 redudant bundle. But the TIM module is not confirable in IM station. Is I need to procure Two different TIM modules? Then How they will be configured at SCADA ? Please let me what will be my new System Configuration?. I am attaching my present system Configuration.
Thanx & Regards, Praveen Patil AttachmentBMF System.pdf (1114 Downloads) |
| 11/13/2007 1:26 PM | |
|
Joined: 9/1/2005 Last visit: 10/31/2025 Posts: 4114 Rating:
|
closed cause question posted twice. The second thread with the subject S7-300 Redundant system Design with Telecontrol module is published within the conference Communication / Networks. Best regards CS Moderator |
|
My Forum is the place to personalize your profile, |
|
Follow us on