(0)| 11/15/2007 11:22 PM | |
|
Posts: 3 Rating:
|
Hi, Belated but thanks for reply. Mean time I was asking all the details regarding same from my client and they provide backup which is openin strucview V 0.1.a. Here I attached one of file for ur ref. Originalfile extension is ENSQN1.CFP I think it is open in STRUC, so if you have any instruction & softwaremanual for this then please forward it to me. Thank you. Gaurav AttachmentENSQN1.pdf (1312 Downloads) |
| 11/19/2007 8:13 PM | |
|
Posts: 3 Rating:
|
Hi, Thanks. It is not a pdf file. You can save that attachment with ‘*.CFP’ extension and open it in strucview software. Here is the attached pdf file for your referance.I have the code with extension *.CFP which is opens in strucview version 1.0.a. This isread only software in which I just read the code. I like to ask you that, 1. Is it open in only STRUC software? 2. Can we convert in D7 Sys software, if yes how & what are the requirements? 3. As per this code, I request you to please send user manuals & instruction manuals. 4. Is it possible to read & modify that code in SIMATIC manager & how? Thank you. Gaurav AttachmentENSQN1.CFP.pdf (1269 Downloads) |
| 11/23/2007 11:44 AM | |
|
Joined: 8/31/2005 Last visit: 12/16/2025 Posts: 2198 Rating:
|
Hello Gaurav, I knew/saw Stucview, but I don't have it. It's not a offical SIEMENS Software. I opened you fíle and saw, STUC 4.2.3 was used for programming. 1. You can "read" it within any Texteditor( orStucview), but to make changes you need STRUC V4.2 2. Yes it's a P32 Prcessor, so you can use the converter to convert it to D7-SYS. You need Step 7, CFC and D7-SYS (But check for correct/matching versions of this software packages before ordering, look here ) How much the converter can do depends on your project, can be 75 to 100%. 3. see here 4. no not only with STEP 7 , you need aditionalCFC (graphical Editor) and D7-SYS (Libary for SIMADYN D / SIMATIC TDC / FM458) |
Last edited by: miami at: 23.11.2007 11:45Last edited by: miami at: 23.11.2007 11:45 |
|
Follow us on