(0)| 1/26/2016 2:38 PM | |
|
Posts: 45 Rating:
|
Dear, I have to connect CP443 with multiple number of Ruggedcom RMC30 MODBUS TCP converters. There is a managed switch X208 between CP443 and RMC30. Please refer attached diagram. CP443 works as MODBUS client while the facilities work as MODBUS servers. The default TCP port number of RMC30 is 502. CP443 should distinguish each RMC 30 by assigning different remote TCP port numbers. That is, CP443 should have different remote TCP port numbers for each connection. My question is as follows. Can I change RMC30 TCP port number from 502? Otherwise, can X208 perform TCP port number conversion? Attachmentdiagram10.pdf (394 Downloads) |
Follow us on