(1)| 2/9/2016 7:08 PM | |
|
Posts: 8 Rating:
|
Hi! I`m using a CPU 416-5H v.6.0.4 with Step 7 5.5 + SP3 to communicate with a Voltaje Regulator DECS-250 Basler. In this net, I have other two equipments: a protection relay (SEL-700G) and a load controller (Woodward). The other equipments are communicating, but with DECS I can`t to estabilish a communication. I created a new software only with the net configuration, without other modules and without other equipments, but I can`t estabilished the communication. I tried communicate with other server (Multicom Beta) and with it I communicated. So, I believe that DECS configuration are ok. It`s follow attached my configuration. The most interesting is that DB_PARAM is freezing: I don`t receive an error and the communication`s parameters aren`t change too. The destination DB is reseted too, but the DECS-250 has some values. If someone has an idea, I`m so thanked. Eduardo Silva AttachmentModbusTCP.zip (437 Downloads) |
Follow us on