(1)| 3/1/2016 12:11 PM | |
|
Posts: 129 Rating:
|
Hi, Check this: On lower side of the page you will find this... Information on successor devices is available by using the following links: - Release for delivery Comfort Panels 49727602 and 60456564 |
Last edited by: PSW2586 at: 3/1/2016 12:15:33 PMLink Edit Last edited by: PSW2586 at: 3/1/2016 12:17:42 PM |
|
| 3/1/2016 5:36 PM | |||
|
Joined: 3/28/2015 Last visit: 12/30/2025 Posts: 727 Rating:
|
Hello, 1-OP27 is replaced by OP270 In this case you should have the original panel program"Protool"and change the device type. 2-The successor of OP270 is OP277 In this case you do the migration from Protool to WinCC flexible 2008 SP2 SIMATIC HMI WinCC flexible 2008 Migration 3-The successor of OP277 is KP700 In this case you do the migration from WinCC flexible to WinCC TIA
|
||
|
Eng.Mohamed Ibrahim |
|||
Follow us on