(0)| 1/25/2008 8:32 PM | |
|
Posts: 151 Rating:
|
Hi ^_^, Did youkeep your PG/PC interface to PC Internal? Regards, SonicRanger |
| 1/29/2008 10:07 AM | |
|
Posts: 1 Rating:
|
I have the same problem (with step7 V5.4 WinaAc 4.1 CP5611) I Tested on two PC (the pc are the same model same configuration) in the first run all well , in the second every time that I run the WINLC with profibus the computer reboot. If I disable the CP5611 card the sistem work (obviusly without I-O) I try many situation but I cannot find why work in the first PC and no in the second .... After i find this ....(Driver for CP5611) Service pack 2 can be downloaded from the download area under entry ID 15341534.
|
Follow us on