(0)| 4/9/2008 2:50 PM | |
|
Joined: 9/27/2006 Last visit: 1/7/2026 Posts: 12479 Rating:
|
Hello kumar; And welcome to the forum. If you are planning to use s7-300 and S7-400 PLCs, I can suggest you look at the following tutorials: https://www.automation.siemens.com/fea/html_76/down_module.htm?HTTPS=REDIR Look at App. 1 and sectionsA and B for starters. If you are looking into S7-200 PLCs, you could look at the following PLC free onlinetraining prepared by Siemens: http://www.sea.siemens.com/step/templates/lesson.mason?plcs:3:1:1 You should make sure you access the latest versions of the software manuals for the platform you are using. They are installed on your computerat the same time asthe programming software, Step 7 (S7-300/400) and Microwin (S7-200). You may also find them on Siemens support website, simply search for them in theProduct Support link at the top of this forum page. There are also demo versions of the softwares (Step 7 Lite for example, good starting place, although it is imited to stand-alone applications, no communications, and Microwin, full time limited version 60 days) that you can use to train on. Hope this helps, Daniel Chartier |
Follow us on