(0)| 4/15/2008 8:25 AM | |
|
Joined: 9/27/2006 Last visit: 1/13/2026 Posts: 12480 Rating:
|
Hello Edmonds; The CP2572 manual Addendum, New Features, v. 8.0, states that the Send/Recieve interface (developped to allow connection with S5 and S7 PLCs)is full-duplex: Active and Passive Partners Send/Receive requires a point-to-point TCP connection between the communications partners. One partner is responsible for initiating the connection request while the other is responsible for accepting or rejecting the request. The partner responsible for initiating the request to establish the connection is called the Active partner. The partner that responds to the connection request is called the Passive partner. To establish a peer-to-peer connection one partner must be Active and the other Passive. NOTE: The connection is full duplex. Once the connection has been established, both partners may use the connection to send and receive data. http://support.automation.siemens.com/WW/view/en/17519012
|
Last edited by: dchartier at: 4/15/2008 8:26 AM |
|
| 4/15/2008 4:34 PM | |
|
Posts: 2 Rating:
|
Thank you. I will look into this. Mike |
Follow us on