9/14/2016 9:00 AM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
To make the program even for a Logo 0BA2 run, the following changes have been carried out: 1.) The block names of some blocks had to be removed because the 0BA2 knows no block name. AttachmentSmall_House_Tmr_OBA2.zip (324 Downloads) |
9/20/2016 1:54 PM | |
Posts: 2930 Rating:
|
Hi, as IXOS mentioned for a LOGO! relay output the load doesn't matter as long as the load is in the valid range (like your lights). One idea from my side. You wrote the second light circuit is with a dimmer. Try to remove the dimmer. Maybe this is the reason why it don't work as it should. Hope this helsp. By the way visit the Siemens LOGO! Internet page. Here you can find examples and also free LOGO! trainings to get familiar with LOGO! |
Follow us on