4/24/2008 7:19 AM | |
Joined: 2/13/2007 Last visit: 8/1/2024 Posts: 20 Rating:
|
Dear Experts, i am very confused assign parameters to an LR200 (7ML54231GB000BB1) in an application of one tank with 3 meters with ice cream. Please see attached picture with distances and the escenary. My doubt is where locate my axis of reference (zero). Radar to low level point of tank or low level point to radar. I have tried of different ways y my true level is not equal to level indicated in the radar. Please, help me to find the following parameters based in attached picture. Low Calibration Point (m) High Calibration Point (m) Sensor Offset (m) Level Offset (m) Thanks in advance, AttachmentLR200 Parametering.pdf (796 Downloads) |
Follow us on