2/14/2017 6:21 PM | |
Posts: 5 Rating:
|
Hello to all, I'm very new to Logo! controller. I'm currently learning how to use this program. I don't have a real hardware Logo!, but I use simulation to check my logic. So far I have made few programs without problems but they all used digital logic (inputs, outputs, AND, OR logic etc.). Now I want to make something with analog values. The program is pretty simple. The user should enter two real numbers from Logo! display, the program would then add these two numbers and then display result as message again on Logo display. So far, I'm not able to do that. Can I upload my program so you can correct it or at least give some useful advice? I'm not sure if during the simulation (F3) keys on real Logo! are simulated with arrow keys on my laptop's keyboard? Thank you in advance. AttachmentTest_display.zip (469 Downloads) |
Last edited by: Has123 at: 2/14/2017 6:34:56 PM |
|
2/14/2017 6:37 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
In attachment is a simple suggestion for your desire. F-keys works only by using webserver or TDE. AttachmentResult.zip (821 Downloads) |
2/15/2017 2:25 PM | |
Posts: 5 Rating:
|
Thank you very much. Tomorrow I expect delivery of my first Logo! PLC module, so I'll be able to make some practical excercise. |
Follow us on