5/28/2008 2:07 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Another way is to addon in Micro Win a PID libraryTry this link: http://support.automation.siemens.com/WW/view/en/18748232 And you will find in the tile of the web page a library for PID. To add a library in Micro-Win software, proceed as follows: 1. Open a new project and go to "File > Add/remove libraries" or click with the right mouse button to"Libraries > add/remove libraries" in the operation tree. 2. Inside the next window go to "Add" and choose the corresponding library. Confirm it with "Save". 3. Confirm the selected library in the next window with"OK". 4. Once having conducted these steps, the corresponding libraries can be found in the operation tree under"Libraries". You can download the three step.zip file "library of PID" for free from the A/M link. |
Ayman Elotaify |
|
Follow us on