4/26/2017 5:59 PM | |
Joined: 1/25/2012 Last visit: 11/11/2023 Posts: 3 Rating:
|
I have used double motor module,but run individual motor in local mode it is vibration and simotion 435 alarm 20005: Device type:1, log.address:1060 faulty. (Bit:0, reason: 0x1h) ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/27/2017 1:07:42 PMNew subject after splitting |
|
4/28/2017 8:09 AM | |
Joined: 9/17/2015 Last visit: 8/1/2024 Posts: 3 Rating:
|
in local mode,certainly simotion can alarm of 20005. it's nothing. exit local mode,you can ack the alarm. |
4/28/2017 8:19 AM | |
Posts: 1529 Rating:
|
SIMOTION will 20005 if you look at it strangely. I actually disable this alarm. Vibration is usually cased by gains being too high. |
Follow us on