7/25/2017 2:13 PM | |
Joined: 8/21/2014 Last visit: 7/31/2025 Posts: 142 Rating:
|
Hi, I have a similar situation like this. I have one ball screw axis which is controlled by two motors(Motors at both ends). I want to permanently gear this two motors/Axis in 1:1 gear ratio. Can I use fixed gearing TO to achieve this? We can call one motor as master and other as slave. Master has a homing routine and positioning feature. In my program, i only give commands to the master motor. I will also gear this master to another axis. On all occasions slave has to synchronously move with master Slave only has to follow master in all motions(whether it's homing/Positioning/Gearing with another axis) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/26/2017 1:56:13 PMNew subject after splitting |
|
7/25/2017 3:29 PM | |
Posts: 1529 Rating:
|
If the two motors are rigidly coupled to each other, you want your slave to be a torque follower of the master, not a position follower. |
Follow us on