12/9/2017 8:04 AM | |
Joined: 7/30/2012 Last visit: 7/23/2025 Posts: 335 Rating:
|
Hello!!!! I'm Using Simotion 410-2DP With S7-300 CPU Everything Works Fine But Sometimes Simotion Goes Stop Mode After That I'm Not Able To Acknowledge From Usual Acknowledge ...It Will Comes Run By PLC Rotary Switch In Simotion LED Showing SF Fault In Simotion Refer Attached Diagnostics File. AttachmentReadTuber.zip (836 Downloads) |
12/11/2017 10:46 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, use substitute values. 7.13.5 Configuration of the I/Os (variables / TO axis) Substitute values for I/O variables page 287 https://support.industry.siemens.com/cs/ww/en/view/109749954 12.1.9 CPU goes to STOP Description If the CPU changes to STOP mode then check the device diagnostics and the alarm window in the SCOUT. The causes of the STOP are entered in the diagnostics buffer. The alarms of the technology objects that can also cause a CPU STOP are displayed in the Alarms window. Possible reasons, why a CPU can go into STOP are: ● Incorrect direct I/O access ● Configuration data access or system variable access to TO if in RESTART (as of V4.1, however, substitute values for system variables are possible; see System variables (Page 135)) ● Missing PeripheralFaultTask (if there is incorrect access to the process image) ● Missing TechnologicalFaultTask (if there are errors on the technology object) ● Processing error in the programs (or missing ExecutionFaultTask) ● Monitoring time overflow of the IPO/servo tasks ● Monitoring time overflow of the BackgroundTask ● Monitoring overflow of a TimerInterruptTask ● Sign-of-life monitoring Simotion - drive ● Technology object alarms with STOP response (e.g. 20001) ● Set mode using system variable https://support.industry.siemens.com/cs/ww/en/view/51786364 |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
12/12/2017 6:54 AM | |
Joined: 7/30/2012 Last visit: 7/23/2025 Posts: 335 Rating:
|
Hello Friends !!! Thanks For Your Replies ....Will Check And Update The Result !!!! |
Follow us on