12/21/2017 8:59 AM | |
Joined: 12/21/2017 Last visit: 7/2/2022 Posts: 4 Rating:
|
Hello! I faced with problem on writing value to Up/Down counter using VM. Details: - I created a small diagram to use this counter as light switch (this is only way i found to control light power using hardware wall-mount impulse button and software modbus switch on HMI). - Linked "Count" parameter to VD10 via "VM mapping" - Started simulation - Saw that VD10 == current count on counter (linking is OK) - But cannot write value to counter in simulation (without any errors) OS Win10 x64 and Ubuntu 16.04. SW version 8.1.1 and 8.2. Questions: 1. What is cause of the problem? 2. Maybe it's possible to solve my task more gracefully? Who can suggest? Thanks in advance! AttachmentCounter.zip (387 Downloads) |
12/21/2017 10:05 AM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35966 Rating:
|
In simulation mode, it is not possible to write to the counter reading via a data table. But in online mode it is possible. AttachmentChanging counter value via Data Table.wmv (421 Downloads) |
This contribution was helpful to
1 thankful Users |
12/21/2017 10:22 AM | |
Joined: 12/21/2017 Last visit: 7/2/2022 Posts: 4 Rating:
|
Got it, thank you! Do you have any suggestion to improve this diagram? |
12/21/2017 10:32 AM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35966 Rating:
|
I do not understand this circuit anyway. That's why I can not offer any improvement. |
12/21/2017 12:27 PM | |
Joined: 12/21/2017 Last visit: 7/2/2022 Posts: 4 Rating:
|
I needed a Pulse relay, but with remote state control from the Network. |
12/21/2017 2:09 PM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35966 Rating:
|
The LOGO! Software already has a ready pulse relay.
AttachmentCounter.zip (365 Downloads) |
12/21/2017 2:25 PM | |
Joined: 12/21/2017 Last visit: 7/2/2022 Posts: 4 Rating:
|
Thank you! |
This contribution was helpful to
1 thankful Users |
Follow us on