(1)| 3/6/2018 11:33 AM | |
|
Joined: 6/5/2009 Last visit: 1/12/2026 Posts: 158 Rating:
|
Dear All, Attached are 2 pictures depicting the system architecture on the PROFIBUS level of communication with the ET200M I/O's and the other consists of MODBUS TCP system. Is it feasible to have multiple MODBUS TCP servers on redundant basis with a redundant S7-400 H station? If so is there any example to describe the connection and the program. Regards, Grim Reaper AttachmentSystem Architecture.zip (370 Downloads) |
Follow us on