6/30/2018 1:23 AM | |
Joined: 9/3/2014 Last visit: 2/13/2025 Posts: 79 Rating:
|
Dear Experts, I need to control next motor, Asynchronous Siemens Motor Reference: 1LA71334AA90-ZN16 Rated voltage: Special voltage, non-standard winding Frequency: 50Hz I've bought a g120 frecuency inverter drive from Siemens that is composed of, a PM 240-2 SINAMICS 6SL3210-1PE23-8UL0, and a CU250-S, I'm trying to control de Motor, but it seems that has a speccial configuration, because It can't reach 20Hz, I've disasembled the motor and I found a diferent rotor, because I think it has two squirrel cage, so I don't know if it needs a special frecuency inverter drive, I've attached a pdf file with the nameplate of the motor and the parts disasembled I will be grateful if you can help me, Thanks in advance, Best Regards,
AttachmentMOTOR.DOC.pdf (343 Downloads) |
7/3/2018 1:51 PM | |
Joined: 9/3/2014 Last visit: 2/13/2025 Posts: 79 Rating:
|
Dear PISCEAN 2010 Thanks a lot for your help, So, I will tell you, Thanks in advance Best Regards, |
Follow us on