(1)| 8/26/2008 6:08 PM | |
|
Posts: 1502 Rating:
|
Do you have a CNC-Maschine (Spindel-Motor ?) If no, what control-Unit are have ? ( Send the "M19" simulation-Code) |
| 8/28/2008 5:49 PM | |
|
Posts: 133 Rating:
|
I may be able to helpyou further alongand I will assume you have a S120 single axis unit with latest version of V2.5 firmware and your induction motor has a pulse encoder with 1024PPR probably and a zero pulse. You will need to go into configuration offline with STARTER and select Basic Positioner for your axis. This enables the functions for EPOS (easy positioning). You will need to turn the positioning mode on and home when you want to position. You may want to set the homing offset to the position you want and then you will be at that postion with a homing command. Attached is an example project using a S120 single axis in vector mode with positioning on an induction motor.The projecthomes off the zeropulse from the HTL encoderand also runs the traversing blocks in EPOS. TheON/OFF command for the drive is the BOP and the positioning mode is selected via binary input. The homing command and traversing blocks are also selected via a binary input. AttachmentEpos.zip (766 Downloads) |
Last edited by: Drives_Coach at: 8/28/2008 5:53 PMLast edited by: Drives_Coach at: 8/28/2008 5:51 PM |
|
Follow us on