(0)| 9/1/2008 5:24 PM | |
|
Posts: 191 Rating:
|
Hi!! first, you have some functions without connection, this works on the simulation, but you wont be able to upload to a LOGO you have many time functions with the same days and start/stop times.. ¿ do you need them as separate time functions ?? maybe you could use only 3 or 4 different time functions and connect them to the AND functions... you have 13 different digital options which start your pump, attached is a program wich shows on the display 4 different inputs, you only have to addapt this to show up to 12 digital signals... 1234 5678 9.10 11.12 hope this helps!! ROSA Attachmentdysplay 4 stages.zip (1113 Downloads) |
| 9/2/2008 12:43 AM | |
|
Posts: 1690 Rating:
|
Hi riiri7707, all answers you are search, i think can you find at die attachment, file "DEMO_view_status_many bits_V1.lsc". I hope the additional filesyou can use too, specialy file "DEMO_flexible_key_inputs_with_scaling.lsc" to inpus yourmodus numbers in a definedrange you can set...(The inputs you not want can be cleared. If you can´t build an circuit ask here again... Best regards Betel Attachment0BA5_DEMOs_for_poll_rush.zip (932 Downloads) |
| 9/2/2008 3:38 AM | |
|
Posts: 191 Rating:
|
Hi!! ¿ what do you mean by "activate manually" ? your modes depend on time and temperature... ¿ do you want to activate a mode even you dont have the time or temperature ? i made a small program to give you an example of what can be done ... it is a little confusing but it is not that hard.. withRIGHT arrow you activate the manual mode withUP anDOWN arrows youmove betwen the number of output you want to change with LEFT arrow you activate a change on the selectedoutput... if you press the RIGHT arrow again you will deactivate the manual mode and your outputs will take their original value. please take a look at it and post if you need further help. ROSA Attachmentmanual mode.zip (870 Downloads) |
| 9/3/2008 12:39 AM | |
|
Posts: 1690 Rating:
|
Hi riiri770, mv answer last night was not in all details correkt and my first solution to manage user inputs to control the modi needs a lot of blocks. Look at the attachment here. I have programmed a version i hope that isyour opinion and i have showed how to integrate this into your program. To full use and simulate correkt, you must add all the parts i have put in at the beginning (modus 1 + 2) and the end (modus 14), but i think that is possible for you. If you have questions about this ask me here.... Berst regards Betel AttachmentDEMO_view_status_many bits_V2.zip (1037 Downloads) |
Follow us on