(0)| 9/12/2008 4:39 PM | |
|
Posts: 102 Rating:
|
Dear Experts, I am using standard PID blocks in my one project. I have confiured 13 PID loops and also cofigured the LOOP_SCHEDUL DB (DB65) as well as FC 2. But some how none of my PID loops are being enable. As per my understanding if I configure the DB as per the manual instruction. the loop activator set the bits through which every PID blocks enables. Also having confusion about CYCLE time. Is Loop schedule FC calculates the CYCLE time of each loop or I have to calculate it? Can u see into the program and tell me what is the missing step. with best regards Dutta AttachmentS7_std_p.zip (595 Downloads) |
| 9/12/2008 5:22 PM | |
|
Posts: 76 Rating:
|
Hi DUTTA , please take a look a this /tf/WW/en/Posts/20991#95177 it may help you. Regards Abdelaal |
Follow us on