(0)| 9/29/2008 3:10 PM | |
|
Posts: 3 Rating:
|
I found the following remark in the PLCSIM-readme.rtf of PLCSIM v5.4
You cannot use S7-PLCSIM with STEP 7 Lite. But then, I can see compatibility matrices that say the opposite. |
| 9/29/2008 3:15 PM | |
|
Joined: 5/28/2008 Last visit: 12/29/2025 Posts: 4522 Rating:
|
Hello ramon.casanova, Iam agree with JMJ. He have sent the matrix compatabilities. and I think that the problem may be with the Microsoft operating system Check the following link http://support.automation.siemens.com/WW/view/en/23642592 Regards, |
|
Ayman Elotaify |
|
| 9/29/2008 3:22 PM | |
|
Joined: 5/28/2008 Last visit: 12/29/2025 Posts: 4522 Rating:
|
Hi ramon.casanova, I think it may be a good idea to use premium studio 2008 software package. As I have understood you need the PLCSIM for a simulation of a small project because you said you are using Step7 Lite. step7 lite normally is used for programming centrallized stations only. In case of networking it could not be covered by S7-lite! So, Premium studio 2008 offers a great siemens software package and it is useful specially if you want to use it for a short time (not more than 14 days!) MLFB: 6ES7815-8CD06-0YA7 PREMIUM STUDIO 2008, DATENTRAEGER (DVD) INCL. TRIAL LICENSE FOR 14 DAYS, E/RT-SW, SW/DOKU. ON DVD, CLASS A, 5 LANGUAGES (G,E,F,I,S), EXECUTABLE UNDER WINXPPROF, WIN VISTA REF.-HW: PC/PG, PCU, S7-300/400, C7 Regards, |
|
Ayman Elotaify |
|
| 9/29/2008 3:39 PM | |
|
Posts: 3 Rating:
|
thanks for the advice about premium studio, |
Follow us on