10/7/2008 5:43 PM | |
Joined: 9/25/2008 Last visit: 10/21/2021 Posts: 8 Rating:
|
This is my trouble… I wan to start and stop engines by local inputs and by remote bits/tags with a WinCC-Flex, the point is that I made this sub routine with this simple circuit but the problem is that when I use the block in more than one network and a start bit is activated, it activates all the engines connected to the different networks Some help please Here the program and picture: AttachmentOn_Off.zip (299 Downloads) |
Follow us on