5/2/2019 2:48 AM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello Shodai; The PLC logic is the least of your problems in this situation. What type of motor do you need to control, is ity 3-phase? Hint: you cannot do this with a single-phase motor. To control the rotation of a 3-phased motor in forward or reverse, you need contactors that will reverse any 2 leads when you want to change directions. See this article for example, it describes the PLC logic involved:. https://www.sanfoundry.com/plc-program-drive-motor-forward-reverse-direction/ These videos can offer ideas on the circuit required: https://www.youtube.com/watch?v=uNygpiG7SGU https://www.youtube.com/watch?v=e03ZFkV8low Hope this helps, |
Follow us on