10/9/2008 12:33 PM | |
Posts: 2930 Rating:
|
Hi, the max is 8 PID-loops. You can program more "by hand" or by "selve made" PID's from www.richtersps.com http://www.richtersps.com/pideasy_S7_200.htm But this only avaliable in German. Multiplexing: this may be a problem because if you want to multiplex two analog IN with one PID-loop then if one analog value is not avaliable the PID will force the OUTPUT to 100%. Regards Helmut |
10/9/2008 1:22 PM | |
Posts: 112 Rating:
|
hi, Thank you for the help, how about multiplexing digital input Sir? Is this have disadvantages? Thanks again |
Follow us on