10/13/2008 9:01 AM | |
Posts: 12 Rating:
|
dear ayman as salam 3alykom it is an existing application and i want to replace the extension cable with longer one the existing extension cable is pin to pin 9 wires cable but i wonder if the PPIprotocol need less than 9 wires it will be oflittle cost thenew distanceis nearly 40 meter plz check the attached pdf of a similar pc/ppi cable (not exact the one i have!!!) and the highlighted text i willtry the 6 pin cable. if not working i will fix the 9 pin cable Regards Mahmoud A.Fattah Attachments7200cableEnglish[1].pdf (713 Downloads) |
Follow us on