5/27/2019 3:47 PM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, are you using SIMATIC S7-31xT controller, like S7-315T or S7-317T(F)? As it is written in the manual, with the function "MC_WriteParameter", you could only write technology parameter on the CPU.
If you want to write drive parameter, use function "MC_WriteDriveParameter". For more information, have a look to chapter 6.8.11. of the manual. |
This contribution was helpful to
1 thankful Users |
5/29/2019 12:47 PM | |
Posts: 241 Rating:
|
thank you |
Follow us on