6/11/2019 12:39 PM | |
Posts: 9 Rating:
|
I it possible to make a program like this in the LOGO! i have made some notes in the zip file, i cant figure out what 'blocks' to use. the light is to be turned on with make contact (I7) this is supposed to turn on the light and start the dynamic light function, (I6) is supposed to stop dynamic light and turn the lights up to max (10V), last the (I5) i supposed to turn off the light. AttachmentDynamic light control.zip (275 Downloads) |
6/11/2019 1:50 PM | |
Posts: 9 Rating:
|
the lux range is 30-3000 Lux 30 = 0 V 3000 = 10 V |
This contribution was helpful to
1 thankful Users |
6/11/2019 2:36 PM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35971 Rating:
|
Here's a possible solution.
AttachmentDynamic light control_V2.zip (278 Downloads) |
This contribution was helpful to
1 thankful Users |
6/11/2019 2:56 PM | |
Posts: 9 Rating:
|
thanks to you, really helpful, to me at least.. |
This contribution was helpful to
1 thankful Users |
6/11/2019 3:00 PM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35971 Rating:
|
Hello Jawdragon, you're welcome. Is your problem solved now with this solution? |
Follow us on