(0)| 7/24/2019 9:30 PM | |
|
Joined: 4/18/2012 Last visit: 12/23/2025 Posts: 41 Rating:
|
Dear Sir Many thanks for your reply, The real problem No exchange data between SIEMENS PLC (CP343) and MOXA gateway. Actually Modbus blocks are not active. whereas I implemented the technical manuals method this document, as below: 1. Installation of "SIMATIC Modbus/TCP CP", Installing the library on the STEP 7 2. I setup the connection parameters in NetPro. 3. Insert the Modbus/TCP blocks in the user project - 4. Calling the Modbus/TCP block FB905 in the required OB 5. Setting the parameter DB Modbus_PARAM_CP according to the requirements with using Modbus TCP wizard 6. I have parameterized the Modbus/TCP block for initialization and for the runtime 7. Downloading the user program to the CPU. I attached project user program and configuration to simplify my question. Thank you very much in advance for your help and support AttachmentConfig and STL Code user program.pdf (433 Downloads) |
Last edited by: S_I&C at: 07/24/2019 21:37:22Last edited by: S_I&C at: 07/24/2019 21:40:50 |
|
Follow us on