8/8/2019 11:38 PM | |
Joined: 3/25/2018 Last visit: 9/2/2025 Posts: 6 Rating:
|
Hello, I have a problem about controlling the two indiction motor with two encoder.Each motor has seperated encoder and encoder module and im using smc30 with drive cliq to D435 .im using _setaxisdatasetactive function for ADS changing .When i change the motors contacts also ADS has been changed , motor has been energized and then when i try to make it move , im getting 7900 : Drive Motor Blocked / Speed Controller at its limit alarm . i think it's because of encoder position information, it is not coming due to changeover process . when i spin it manually, encoder information is coming OK.i check it over sensordata[] parameter. i've changed the number of encoders data from axis's expert list.my first encoder number is 1 other one is 2.When i change the motor's contacts , data set monitoring shows actual data set that is correct parameter.But i think i'm doing wrong something on changing process .i attached the some screenshot about problem. is there any solution about this problem ? [snip[
AttachmentScreenshots.zip (376 Downloads) |
Last edited by: Aykute at: 08/08/2019 23:40:22Last edited by: Aykute at: 08/08/2019 23:42:46Last edited by: Aykute at: 08/08/2019 23:43:00Last edited by: Aykute at: 08/08/2019 23:51:17Last edited by: Jen_Moderator at: 08/09/2019 07:47:48Removed links and added files as an attachment. |
|
Follow us on