5/3/2017 11:28 AM | |
Joined: 10/1/2013 Last visit: 9/1/2025 Posts: 605 Rating:
|
Hi Nohuman, the RF180C V1.1.0 works just fine with the "Ident Blocks" (but you have to project a RF180C V2 in TIA). Nevertheless I'd recommend to update the module because it's only guaranteed to work with FW 2.2.0 or higher combined with the ident blocks. Make sure your RF180C's hardware version is 7 or higher before updating. If your RF180C's version is lower then 7 you won't be able to upgrade to FW >2 . In this case you need to buy a new module or contact your sales man for upgrading your module. Another option is to use FB45 with an old module, as you mentioned before. Documentation: |
Last edited by: Owei at: 5/3/2017 11:29:44 AMLast edited by: Owei at: 5/3/2017 12:36:47 PMLast edited by: Owei at: 5/3/2017 12:37:13 PM |
|
This contribution was helpful to
1 thankful Users |
5/3/2017 4:40 PM | |
Joined: 2/22/2016 Last visit: 9/25/2022 Posts: 9 Rating:
|
Hi Owen, How can I know the version of RF180C? If is it version 7 ? o lower |
1/18/2020 8:55 AM |
|
Posts: 4 Rating:
|
YAA |
Follow us on