2/27/2020 6:48 PM | |
Posts: 2 Rating:
|
TIA Portal V13 SP1, Scout 4.5, Yes recompile, Copy paste method, we want to collect data from running machines. We want to show 4 simotion tags in one hmi. |
2/28/2020 11:06 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello does the single connection to each simotion work? if not --> first of all prefere upgrade V13 to SP2 https://support.industry.siemens.com/cs/ww/en/view/89331880 Independent from some restrictions you also can collect data from the each other CPU's only in one SIMOTION which is connected to HMI. Communication mechanism between other SIMOTION-CPU's could be I-device or TCP/IP (using Library LCOM, very easy to realize) or OPC-UA .
|
With best regards, |
|
Follow us on