(0)| 4/27/2006 4:52 PM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, regarding to your inquiry we would like to inform you. It is possible that your installed software package STEP 7, optional packages (S7-GRAPH, S7-PDIAG, CFC...) together with the Windows 20003 is not compatible. Please see the home page of the SIMATIC customer support and find the following FAQ which do you will find by the quoted Beitrags-ID: http://www.siemens.com/automation/csi_en/product FAQ: "Compatibility of STEP 7 versions with the MS Windows operating systems"by Entry ID: 8250891 Consider: STEP 7 V5.3 incl. SP2 is not enabled for use inMS Windows Server 2003 incl. SP1. MS Windows Server 2003 as a workstation computer, STEP 7 V5.3 SP2 is required. Please see also theFAQ: "Compatibility list for SIMATIC software packages with STEP 7 V5.3" by Entry ID: 18734363. With best regards Cicero |
Follow us on