(0)| 12/23/2008 4:46 AM | |
|
Posts: 11 Rating:
|
Hi, I got problem when using the 420 demo Case with computer, I use USB to com port to link them together. I set the computer and the device as the FAQ "My PG/PC has only USB com-ports. How I can get online with my drive?", the baud rate of 9600 and 38400 had also tried. There is a error ret:0xbe0b0028 shown on the starter program. I have test the Serail port there are signal at the tx pin with corrert frequecny as the baud rate set. I'd like to know how to solve the problem? Thanks |
| 12/23/2008 6:54 AM | |
|
Joined: 3/21/2006 Last visit: 1/8/2026 Posts: 10247 Rating:
|
Hello Antony Lau, Are you sure that use up-to-date drivers for USB to Serial? And also up-to-date Starter ? Try also with reinstall of Starter program... regards |
This contribution was helpful to
|
|
| 12/29/2008 2:54 AM | |
|
Posts: 11 Rating:
|
Thanks a lot, problem solve |
Follow us on