(0)| 1/7/2009 4:04 AM | |
|
Posts: 100 Rating:
|
Hi to all Now i control micromaster 440 through profibus.the MM440 used for high pressure pump. I SET IN BOP RAMP UP TIME 20SEC RAMP DOWN TIME 40SEC I am using 2wire control method. i attached the diagram below. The High pressure output in Q4.7. The high pressure output connected to MM440 5th & 9th terminal. When the high pressure pump on MM440 get supply.i switch on the drive ready commend(profibus control) while high pressure pump on.i attached the diagram below. I give constant power supply to main supply of MM440. MY QUESTION IS IF I SWITH OFF THE HIGH PRESSURE PUMP Q4.7. THE MM440 DON'T GET SUPPLY IN THAT TERMINAL. (5&9) DOES NOT CLOSE 1.WHEATHER THE HIGH PRESSURE PUMP IMMEDIATLY OFF OR AFTER 40 SEC(RAMP DOWN TIME) 2. IF IMMEDIATELY OFF MEAN WHAT I SHOULD DO FOR RAMP DOWN. Attachment2WIRE&HP.zip (279 Downloads) |
| 1/7/2009 5:28 AM | |
|
Posts: 217 Rating:
|
Dear sunder, I think to my knowledge if you are using ON/OFF1 for digital input 1(terminal 5, P701=1). After you give signal ON it’ll start with ramp up and when you disconnect input it’ll stop with ramp down. But I think you are using profibus so you can take that input to PLC and you can start/stop MM440 through profibus. For that it will be useful this link. I hope this will help you. Regards. |
| 1/7/2009 9:13 AM | |
|
Posts: 100 Rating:
|
thanks The drive control terminal get input from PLC output. using profibus i control the speed of the motor.i didn't go to commisioning yet.this is my first project in drives. i set the parameters what i attached below. if there is any modification pls help me to rectify. i set the parameters using my attachment information. your setting should also allow the speed control (using profibus). pls send me the modified value in change column in my attachment. Attachmentdrive setting.zip (305 Downloads) |
Follow us on