(0)| 9/27/2020 9:55 AM | |
|
Joined: 9/2/2020 Last visit: 5/3/2025 Posts: 62 Rating:
|
Hi I worked on machine without changing motor. Now the axis works but has a problem, it means that I have over shoot in the motor operation then there is a big Knock at the both ends of Knife Axis. I think I should change the parameters of PI control but from where exactly? and second note is that in my project parameters are not on my hand and is changed from profibus network. how can change access? When I change parameters (like Gain P_gain or Reset time in PI controller of drive) the Error massage 1 comes.(first picture of attachment) and sometimes i have the second picture. Summary: How can i tune the motor for normal behavior? Best regards AttachmentNA-ABer.pdf (882 Downloads) |
Follow us on