11/10/2020 5:26 PM | |
Joined: 9/8/2020 Last visit: 2/14/2024 Posts: 7 Rating:
|
Hi, I have a major problem with the IOT2050. I was trying to write the image to the internal memory using the following command: dd if=/home/IOT2050_Example_Image_V1.0.2.imgof=/dev/mmcblk1 At that moment I was using the OS which was already installed on the internal memory. Normally this procedure should be done while booted from an usb drive. I haven't done this. Now I can't get it to boot. I think it should be possible to unbrick the IOT2050 using the u-boot. But oddly enough I can't get into it. My keyboards are only recognized AFTER the u-boot "press any key to interrupt the boot" countdown. How can I solve this situation? This is the serial output. When the IOT2050 reaches kernel panic, the STAT led stars blinking red.
Kind regards, Diederik Vermeersch Attachmentoutput.txt (615 Downloads) |
Last edited by: Jen_Moderator at: 11/11/2020 09:23:18Added output as txt file. |
|
Follow us on