(0)| 12/4/2020 1:06 PM | |
|
Joined: 12/12/2016 Last visit: 12/11/2025 Posts: 640 Rating:
|
Hello, The iot2000setup tool currently only supports wpa-psk setup, as we can see how the /etc/wpa_supplicant.conf is configured (check line 65). On the other hand, a manual configuration of this file could be done like this:
Then enter the details of your WPA2-enterprise configuration:
-> Notice that you will have to copy the RADIUS certificate to a location on the IOT2040 as mentioned above: ca_cert="/etc/certs/radius.pem". If you have no clue where to get this certificate, try leaving this line out first, depending on how your company router is configured you might not need it. Afterwards edit /etc/network/interfaces and add the wlan0 interface (for the USB-Dongle or mPCIe Card you are using)
Then restart the network connection:
Hope this helps!
|
This contribution was helpful to
|
|
Follow us on