10/16/2007 8:52 AM | |
Posts: 12 Rating:
|
How do i establishe communication between simotion d445 and wincc via ethernet? |
10/24/2007 6:45 PM | |
Joined: 10/24/2005 Last visit: 11/14/2024 Posts: 14 Rating:
|
With WinCC Scada or WinCC Flexible? Because with WinCC Scada I think it is not possible because you don't have the Simotion Protocole inside. But with WinCC Flexible just add a new "PLC" with the IP adress of the Simotion unit and use the Simotion Protocole. In attachment you have the compatibility software file for Simotion Scout V4.1 SP1 and there is no reference for WinCC Scada! Have a nice day, Denis. AttachmentCompatibility_SIMOTION_V411_76.pdf (817 Downloads) |
9/5/2008 10:03 AM | |
Posts: 7 Rating:
|
any answer ? |
12/20/2008 2:17 PM | |
Posts: 7 Rating:
|
I am trying to interface with ethernet and the WinCC scada over Simtic Net OPC to a C230. |
12/20/2008 7:55 PM | |
Posts: 7 Rating:
|
I am trying to get my C230 communicate to WinCC Scada over ethernet using the Simatic Net OPC. I am having issues having the OPC Scout get online with the C230 over ethernet. I can ping the C230 good. I have Scout 411. and Simatic Net OPC ver 7.0. The tags are exported and I can see them, but they will not go online. Any help or comments are appreciated. Bryan bstueben@appliedc.com |
Follow us on