12/29/2020 3:21 PM | |
Joined: 12/27/2018 Last visit: 4/1/2025 Posts: 4 Rating:
|
Hi, I have a problem running the MB_CLIENT block which has something to send. If I manually modify the bit that starts the transmission, the transmission will be performed correctly. If I let this be done by application logic, the data will not be transferred. I noticed a strange behavior of the MB_CLIENT block for me. In the case of manual modification, the transfer takes 90ms (manual.png), when it is done, the application takes 45ms (program.png). Description: Network20: evaluates the difference and sets the bit to perform the preparation. Network21: sets variables and sets a bit to transfer data. Network22: MB_CLIENT is activated, resets bits after transmission. Could someone smarter explain this behavior to me, or alert me to where I'm making a mistake? Thank you for any help. Lumirt
Attachmentsample.zip (609 Downloads) |
Follow us on