3/20/2018 12:23 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello Jackcaress, This post should have publsihed in SIMODRIVE Converter system product conference since the MLFB number is of 611 drive control card. From the MLFB number it is dual axis control card with resolver feedback with standard interface. Please refer attached sheet for pin layout details of X311 & X321. HTH |
This contribution was helpful to
1 thankful Users |
3/20/2018 12:46 PM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
Is there a manual or document for this control card because i need to know the inputs of the cables that are connected (Photo) |
Last edited by: Jackcaress at: 3/20/2018 1:00:00 PM |
|
3/20/2018 1:11 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, The TOP X321 & X322 - terminal numbers 56 & 14 are 0.. +/- 10V analoge speed setpoints for 2 separate axes. Bottom terminal number 9 & 663 are pulse enable. Do you have electrical wiring connection diagram of the card? If yes, please attach so better terminal discription could be inform. |
3/20/2018 1:37 PM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
This is the wiring diagram from the machiene manual |
3/20/2018 1:39 PM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
|
3/21/2018 4:33 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, 6SN1123-1AB00-0BA0 is dual axis power module configured to power X & Z axes motors in your case. X AXIS From Fagor X8 connector pin number 1 & 9, analog 0 to +/- 10 Volt is fed as set point to Siemens 6sn1118-0bk11-0aa0 control card connector X321 terminal 56 & 14. X331 terminal 9 is 24 V potential output for pulse & controller enable. X331 terminal 663 is pulse enable & X332 terminal 65.1 is controller enable. Z AXIS From Fagor X8 connector pin number 2 & 10, analog 0 to +/- 10 Volt is fed as set point to Siemens 6sn1118-0bk11-0aa0 control card connector X322 terminal 56 & 14. X331 terminal 9 is 24 V potential output controller enable. X332 terminal 65.2 is controller enable (2nd axis) Please check X axis pulse enable & controller enable signals are healthy & with the set point value, motor should run. Also I suggest you to check the motor encoder cable continuty connected to Fagor X1 connector . HTH. |
Last edited by: PISCEAN 2010 at: 3/21/2018 4:37:29 AM |
|
This contribution was helpful to
2 thankful Users |
4/27/2018 10:19 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, I found the manuals on Siemens web. Please refer the link below which may be useful to you in future. SIMODRIVE 611 analog, Start–up Software for Main Spindle and Induction Motor Modules Version 3.20 SIMODRIVE 611 analog, Transistor PWM Inverters for AC Feed Drives and AC Main Spindle Drives |
Follow us on