7/24/2007 10:05 PM | |
Posts: 191 Rating:
|
Hi!! some times simple things work better than breaking your mind trying to do something complicated.. please analize the program i´m attaching.. it is a diferent approach than the one you were asking for, but i think it works fine.. when you are recirculating it allows to start the acid pump. if the PH is higher than the SP the acidpump wil run for XX sec ( xxxml ) and then it will wait for YY min, if the PH is still higher than te SP the acid pump will run for other XX sec. if the SP is lower than the SP the acid pump will not run. this ensures that you reach the desired SP adding only the acid needed in increments of xxxml you must set a YY time large enough to allow the acid to react with watter, but short enough to reach the desired SP in the time you have the recirculating pump on. i´ll look for your comments. ROSA AttachmentPH.zip (732 Downloads) |
This contribution was helpful to
1 thankful Users |
7/26/2007 5:01 AM | |
Posts: 191 Rating:
|
Well it is amazing, but it is posible to do what you want!!! belive me....ifi´d chrge you for this it would be very expensive... ( at least a BBQafter swimming) there are only 4 values you must change ( they are in magenta in the program ) 1.- the base time for the 1st sample 2.-the set point 3.- thesteady time ( waiting for the 1st acid to work) 4.- the same base time you used for 1st sample ¿¿ how does it works ?? well not everything is thatsimple... please sudy it and post your specificdoubts hope this helps!! ROSA AttachmentPH amazing.zip (699 Downloads) |
This contribution was helpful to
1 thankful Users |
7/26/2007 10:42 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi, perhaps it can help you, i attached a sample for a easy wayto memory analoge values. In the sheed the minimum and the maximum of an analoge Input / value was memoried... Kind regards, Betel AttachmentTEST_Speicherung_von_analogen_Werten_mittels_Multiplexer.zip (648 Downloads) |
==> Meine TAG-Listen: "deut." |
|
Follow us on