9/23/2022 11:09 AM | |
Joined: 3/25/2008 Last visit: 9/17/2025 Posts: 224 Rating:
|
just a note the minimum cable length between two participants is 1m
|
9/26/2022 9:42 AM | |
Joined: 3/27/2008 Last visit: 9/14/2025 Posts: 1216 Rating:
|
Akash I understand the production is now working which is good, whilst there are some issues with this enclosure, the main this is to get production going. I have attached a pic of a new panel, which shows how these interconnections can be achieved for future installations, which may also help other Engineers who have to manage operation with inverter drives. Tractor Attachmentscreening within the enclosure short.pptx (889 Downloads) |
Tractor |
|
9/26/2022 9:59 AM | |
Joined: 3/27/2008 Last visit: 9/14/2025 Posts: 1216 Rating:
|
A further pic. to show internal motor cables exit from top of enclosure, there is a limit of upload here. Tractor Attachmentscreening output motor cables.pptx (751 Downloads) |
Tractor |
|
10/10/2022 4:04 AM | |
Joined: 9/8/2022 Last visit: 7/5/2024 Posts: 10 Rating:
|
Sir, That's my network current status |
Follow us on