1/13/2019 2:14 PM | |
Posts: 12 Rating:
|
Thanks to nulizhang! Your answers really helped me in configure the drives. Now I can set commands to the drive and received status info from the drive. Highly appreciate the help info from the forum! Also thanks to the mediator who organized topics very well! My next question is who know more on how to fine tune a Siemens drive for a spindle motor? Especially if I do not have enough information on motor and encoder. Here is the detail: Drive P/N: 6SN1123-1AA00-0LA1 (p/n is verified) Analog plug-in board P/N: 6SN1118-1NH01-0AA0(p/n is verified) Spindle motor:1PH2095-6WF41 (p/n cannot be verified, because cannot be seen) Motor encoder: 256 pulses/rev, sin/cos 1Vpp (p/n cannot be verified, because cannot be seen. When sending encoder signals in TTL from the drive interface board to CNC, I got 1025 pulse per motor revolution.) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/14/2019 12:12:33 PMNew subject after splitting |
|