3/21/2017 9:25 AM | |
Joined: 2/20/2014 Last visit: 9/3/2025 Posts: 405 Rating:
|
Hi, I have connected one Ethernet cable from IOT 2040 to my laptop & another Ethernet cable from IOT 2040 to the wifi router but when i try to ping using "ping www.google.com", i only get the following: "ping: bad address 'www.google.com'". Can anyone here advise me on how i can make a successful internet connection to the IOT 2040? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/21/2017 3:07:43 PMNew subject after splitting |
|
3/21/2017 9:40 AM | |
Posts: 71 Rating:
|
Is DHCP enabled for the port you use to connect to the router? Use iot2000setup to check and/or reconfigure. |
This contribution was helpful to
1 thankful Users |
3/22/2017 8:46 AM | |
Posts: 531 Rating:
|
dns 8.8.8.8 as DNS Server to the ip setting does not help? |
This contribution was helpful to
1 thankful Users |
3/22/2017 10:11 AM | |
Joined: 2/20/2014 Last visit: 9/3/2025 Posts: 405 Rating:
|
tried already, same as earlier unable to ping www.google.com |
3/22/2017 11:01 AM | |
Posts: 531 Rating:
|
What happens if you use the ip itself. Ping on another pc and use that google ip adress to check whether dns resolving is the problem or something else. |
3/22/2017 11:02 AM | |
Posts: 531 Rating:
|
If it is dns related, you can try to ping on pc and take the ip address and ping with that instead of google.com on the IoT 2040. |